| Date Posted | Question |
02/28/2013 | I am using the MOP function on the 7 series drives and on my deceleration; the drive is following the speed pot instead of the deceleration time. Why is that? |
09/13/2012 | How do I order touch up paint? |
08/31/2012 | When reading 42h it does not match U1-03? Using Ethernet or Modbus protocols. |
08/28/2012 | What are the main causes of the VCF/VCN alarm? |
11/16/2009 | Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? |
06/08/2007 | Can multiple motors be used with a single inverter? |
11/28/2005 | What will happen if there is only .5'' clearance from either top or bottom of the drive to an enclosure? |
11/28/2005 | If the drives carrier frequency is changed , is it necessary to re-autotune the drive?
|
10/28/2005 | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |
10/27/2005 | Does installation of an AC Drive near a large capacitor bank (power-factor correction) require special consideration? |
10/21/2005 | What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display? |
07/13/2004 | Resetting a drive fault. |
07/13/2004 | What is the meaning of CAL or CALL on the keypad display?. |
07/13/2004 | Is it possible to adjust the brightness for the operator display? |
07/13/2004 | Is it possible to use auto-tuning without rotating the motor? |
07/13/2004 | What is the ambient temperature derating (L8-12 setting)? |
07/13/2004 | What are some counter-measures to reduce harmonics created by AC drives? |