| Date Posted | Question |
06/19/2013 | How do I re-allocate a digital input on a DI-100 or DI-101? |
02/28/2013 | How do I get a 0-20mA signal out of the analog outputs? |
02/28/2013 | How do I save and recall parameter settings for User Initialization? |
02/28/2013 | How do I create a User-Set scaling in the 1000 series drives? |
02/28/2013 | I am using the MOP function on the 7 series drives and on my deceleration; the drive is following the speed pot instead of the deceleration time. Why is that? |
02/28/2013 | I am writing to the speed reference register using MODBUS TCP/IP for my 1000 series drive, yet U1-01 does not read properly. I can write to other registers with no problem. What are my possible issues? |
11/30/2012 | are the digital outputs able to be inverted |
10/30/2012 | How to change motor direction when rotating backwards? |
10/29/2012 | During Start up, my drive injects a max speed into the motor, then OL2 is returned. How do I prevent this? |
10/09/2012 | When using 2 option cards, I am receiving an OPE06 fault and am not seeing all the F1 parameters. I am using CN5-B for my encoder feedback card. |
08/28/2012 | Hbb fault occurs with the H1,H2 and HC jumpered, what else could the issue be? |
08/17/2012 | Are adaptor plates available for mechanical mount retrofitting of F7? |
05/31/2012 | Will the A1000 be part of the configured drive program? |
05/31/2012 | Are end caps (NEMA 1 kits) available for the protected chassis versions? |
05/30/2012 | What are the details regarding A1000 12 Pulse? |
02/29/2012 | Does the A1000 have a USB cable interface (instead of serial) for direct connection to a computer, and do I need anything else? |
02/08/2011 | What do I do if I am having problems connecting to the A1000 USB port? |
01/04/2011 | What are the differences between the A1000 600V and A1000 240/480V models? |
01/04/2011 | What are the A1000’s ratings? |
01/04/2011 | Where does the A1000 fit into Yaskawa’s family of drives, and what does it offer beyond the F7? |
01/04/2011 | Is the A1000 dual rated? |
01/04/2011 | Where is the A1000 manufactured? |
01/04/2011 | Are F7 Options compatible with A1000? Can A1000 Options be used with F7? |
01/04/2011 | Is the product ready for shipment? |
01/04/2011 | In Normal Duty mode, is the default carrier frequency higher than 2kHz? |
01/04/2011 | What control methods does the A1000 offer? |
01/04/2011 | Can we replace simple servo applications using existing PM servo motors? |
01/04/2011 | How can the design life of the A1000 be twice that of the F7? |
01/04/2011 | What is the scan rate of the A1000? |
01/04/2011 | Is the A1000 the same physical size as F7? |
01/04/2011 | Are the A1000 network communications full function Modbus or Yaskawa standard? |
01/04/2011 | What is EN61800-5-1 and TUV? |
01/04/2011 | What will happen to the F7? |
01/04/2011 | Will there be a remote keypad option? |
01/04/2011 | Will DriveWizard Industrial be backward compatible? |
01/04/2011 | When should we begin converting existing F7 business to A1000? |
01/03/2011 | When will the rest of the A1000 600V models be released? |
01/03/2011 | What tools are available to help customers convert from G5 (600V) and F7 to A1000? |
01/03/2011 | When will end caps (NEMA 1 kits) be available for the protected chassis versions? |
01/03/2011 | Can the 600V models be used with a 690VAC input voltage? |
01/03/2011 | What is RoHS? |
01/03/2011 | What A1000 enclosure types are available? |
01/03/2011 | What training is available for A1000? |
01/03/2011 | When will single phase input capacities be available for A1000 and what kind of derating is expected? |
01/03/2011 | What documentation ships with the product? |
12/21/2010 | Are there plans for a dedicated 600V micro-drive? |
12/21/2010 | After installation of DriveWizard Plus on a Dell PC, the following Windows error is displayed when attempting to launch the application: "The application failed to initialize properly (0xc000007b). Click on OK to terminate the application" |
11/28/2005 | If the drives carrier frequency is changed , is it necessary to re-autotune the drive?
|