| Date Posted | Question |
02/28/2013 | How do I save and recall parameter settings for User Initialization? |
02/28/2013 | How do I create a User-Set scaling in the 1000 series drives? |
02/28/2013 | I am using the MOP function on the 7 series drives and on my deceleration; the drive is following the speed pot instead of the deceleration time. Why is that? |
12/29/2012 | How do I create a Device ID in bacnet? |
11/26/2012 | How do I set up a simple PID loop on a Z1000/Z1B? |
11/26/2012 | Can you explain the Hand/Auto Mode selection on the Z1000 series? |
11/02/2012 | oPE08 occurs after I lower L6-02, why is this? |
10/29/2012 | During Start up, my drive injects a max speed into the motor, then OL2 is returned. How do I prevent this? |
09/13/2012 | Where is the Z1000 manufactured? |
09/12/2012 | Is Apogee/Metasys available for the Z1000 & Z1000 Bypass |
08/28/2012 | I have OL2 alarms at start up, when I look at the fault trace history, I see a output frequency of greater than 50 Hz, what could be causing this? |
08/21/2012 | What is +P common |
06/29/2012 | What is RoHS? |
11/29/2011 | What documentation ships with the product? |
11/29/2011 | What will happen to the E7? |
11/29/2011 | Are there plans for a 600V Z1000 drive? |
11/29/2011 | Are E7 Options compatible with Z1000? Can Z1000 Options be used with E7? |
11/29/2011 | What new features does the Z1000 offer beyond those of the E7? |
11/29/2011 | Is the Z1000 the same physical size as E7? |
11/29/2011 | What are the Z1000 ratings? |
11/29/2011 | When should we begin converting existing E7 business to Z1000? |
11/29/2011 | Will there be a remote keypad option? |
11/29/2011 | Will the Z1000 improve startup times in the field? |
11/29/2011 | What tools are available to help customers convert from E7 to Z1000? |
11/29/2011 | Does the Z1000 have a USB cable interface (instead of serial) for direct connection to a computer, and do I need anything else? |
11/29/2011 | What DriveWizard program does it use, and is it backwards compatible with E7? |
11/29/2011 | What are the embedded network protocols for the Z1000? |
11/29/2011 | When will a heatsink through the back solution be available, and what enclosure rating will it be capable of? |
11/29/2011 | What Z1000 enclosure types are available? |