Global Sites
Home
Site Map
Contact Us
Search
Advanced Search
Partner Info Login
Home
>
Downloads/FAQs
> Search Inverter Drives FAQ Knowledgebase
Search FAQ Knowledgebase for Inverter Drives
To find an FAQ in our FAQ Knowledgebase, select one of the search options below. Enter your search terms into one of the forms and select the search button in that form to perform the search.
Search by Product
Use any or all of the fields below for the document details search.
Product:
(Use ctrl & click to multi-select)
-Select-
A1000 Configured
A1000 Drive
AC Motors
AC7 Matrix Converter
Any AC Drive
Bypass Unit
DC5 Converter
Drive Options
DriveWizard Plus Software
DriveWizard Software
E7 Drive
E7B Drive Bypass
E7BR Package
E7C Drive Configured
E7CR Package
E7E Drive Engineered
E7L Drive Bypass
E7N Narrow Bypass Package
E7S Slim Configured Package
F7 Drive
G3 GPD503 Drive
G5 Drive 600 Volt
G5 GPD515 Drive
G5HHP Drive
G7 Drive
GPD505 Drive
H5 Drive
iQpump 7 Series
iQpump1000
J1000 Drive
J7 Drive
L1000A Drive
L1000V Drive
Network Comms-APOGEE FLN
Network Comms-BACnet
Network Comms-DeviceNet
Network Comms-EtherCAT
Network Comms-Ethernet
Network Comms-Lonworks
Network Comms-Metasys N2
Network Comms-Modbus
Network Comms-Profibus
Network Comms - Landis FLN
Network Communications Options
P1000 Configured
P1000 Drive
P5 Drive 600 Volt
P5 GPD506 Drive
P7 Drive
P7B Drive Bypass
P7BR Package
P7C Drive Configured
P7CR Package
P7S Slim Configured Package
PS5 Drive
R3 Drive
RC5 Converter
SS5 Drive
V1000-4X Drive
V1000 Drive
V7 Drive
V74X Drive
V7C Package
V7CX Package
V7N-4X Drive
V7N Drive
VCD723 Drive
VG3 VCD703 Drive
VH3 Drive
VS mini
Z1000 Bypass
Z1000 Configured
Z1000 Drive
Application:
(Use ctrl & click to multi-select)
-Select-
Aerospace
Aggregate
Agriculture
Automotive
Building Automation
Cement
Centrifuge
Chemical/Petrochem
Coating
Collating
Converting
Conveyor
Depalletizer
Dynamometer
Electronics
Elevator
Elevators and Escalators
Escalator
Extruder
Fans & Pumps
Feeder
Food and Beverage
Forest Products
General Machinery
Glass
Grinder
HVAC
Indexing
Irrigation
Knitting
Lathe
Laundry
Machine Tool
Material Handling
Metal Forming
Metals
Mining
Mixer
Oil Gas and Petroleum
Oil & Gas
Packaging
Palletizer
Paper
Pharmaceutical
Plastics
Plastics and Rubber
Positioning
Power
Printing
Pulp & Paper
Pump Systems
Punch Press
Rubber
Semiconductor
Steel
Sugar & Alcohol
Textile
Transportation
Washdown
Water and Pumping
Water & Waste Water
Winder
Wire and Cable
Woodworking
Category:
(Use ctrl & click to multi-select)
-Select-
Adjustments
Alarm
Application Example
Applications
Braking
Bypass Function
Circuit Protection
Dimensions
Document Clarification
Drive Size
Drive Wizard
DriveWorksEZ
Dynamic Braking
Enclosure
Environment
Fault Code Description
Harmonics
Inputs / Outputs
Installation
Instructions
Isolation Transformers
Keypad-Operator
Lead Length
Maintenance
Motors
Network Communications
Networks
Operation
Options
Parameters
Parts or Replacement
PID Application
Power Quality
Product Launch
Programming
Protective Features
Reactors
Reliability
Service
Software
Specifications
Speed Control
Start up
Starting/Stopping
Training
Troubleshooting
Tuning
Wiring
Search by Keyword
Type in a word or phrase:
Top 10 Frequently Asked Questions:
1.
Can the G5 GPD515 drive in flux vector mode can run above 1750 RPM/60 Hz. If so what parameters would need to be changed to accomplish this. We only want to go to 2100 RPM/72 Hz.
2.
What is the cable pin out for the following cable. P/N uwr00103-1 for used with the Drive Wizard ?
3.
If the drives carrier frequency is changed is it necessary to re-autotune the drive?
4.
Can the keypad from J7 Drive be removed and installed at a remote location? If yes what is the part no. of the cable and what is the distance it can support?
5.
Can the brake coil of a brake-motor be put directly across the motor winding when the motor is run by a VFD?
6.
What are the concerns when operating a motor with a AC drive rated for less output voltage than the motor namplate . Example: The AC drive rating is 480 VAC and the motor is 600VAC.
7.
Is it possible to control multiple motors from a single AC drive?
8.
Is PID available on the J7 Drive?
9.
Can the PID in the V7 Drive be used for positioning?
10.
In some pumping systems the motor speed is normally about 80% of rated motor speed. However periodic purging of the pumping system requires the pump to go to full speed for a while then return to normal. How is this done with the V7 Drive?
Search Downloads
Inverter Drives
Spindle Products
Servos
Controllers
Browse Downloads
Inverter Drives
Spindle Products
Servos
Controllers
Search FAQ
Knowledgebase
Inverter Drives
Servos & Controllers
Submit Inquiry
Literature